This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMS320F2808: F2808 flash API: Programming consecutive flash sectors with a single program action

Expert 5575 points

Replies: 3

Views: 120

Part Number: TMS320F2808

Hi expert,

For F2808 device, could Flash2808_Program function program consecutive addresses across the boundary of two flash sectors?

I didn't see any limitation from the guide book.

BTW, I'd like to double confirm if F2803 device should use F2808 API.

Thanks

Sheldon

  • Hi Sheldon,

    Sheldon He
    For F2808 device, could Flash2808_Program function program consecutive addresses across the boundary of two flash sectors?

    Yes, you can program across flash sector boundaries.

    Sheldon He
    BTW, I'd like to double confirm if F2803 device should use F2808 API.

    This is not correct. The F2803x should use the respective Flash API within C2000ware. Located at the below:

    C:\ti\c2000\C2000Ware_2_00_00_02\libraries\flash_api\f2803x

    Best,

    Kevin

  • In reply to Kevin Allen18:

    Hi Kevin,

    Thanks for your information. BTW, I do mean the special part number which is not a Piccolo device but belongs to F2802, F2806, F2808, F2809 series.

    Could you help me with this?

    Thanks

    Sheldon

  • In reply to Sheldon He:

    Hi Sheldon,

    Sheldon He
    BTW, I do mean the special part number which is not a Piccolo device but belongs to F2802, F2806, F2808, F2809 series.

    Sorry, you were right. It will use the same flash API as the F2808 and its family (F280x). The names being so similar catches me off sometimes.

    Best,

    Kevin

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.