This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: TMS320F28335 UPGRADE

Part Number: TMS320F28335
Other Parts Discussed in Thread: TMS320F28388D, TMS320F28386D, TMS320F28384D, TMS320F28378D, TMDXCNCD28388D, TMS320F28379D

Tool/software: Code Composer Studio

Hi:

We have a control solution based on the 2 single core TMS320F28335 DSPs, it works fine but we are running out of space to implement new features, so we need to upgrade to DSP to a bigger versión, if possible we will like to add some communications such as Ethernet.

Also it is very important to reduce the number of componentes using maybe a dual core microcontroller and also to keep as much as possible the compability of the old code with the new DSP, I have been looking around de TI site and the most powerfull devices based on the DSP C28x are C2000 Delfino microcontollers such as the TMS320F2838x FAMILIY, for example:

  • TMS320F28388D
  • TMS320F28386D
  • TMS320F28384D

When are they and their evaluation kit going to be available?

In case they are not available soon what is the best dual core current option? TMS320F28378D?

Best Regards.

Kepa.