Hello everyone,
I am designing a board for an F280049. Doing so I also take a look at the ControlCard Schematics that TI provides. In case of the mentioned Piccolo there are several 330pF capcitors directly connected to the analougue inputs at the control card. I usually work with the Delfino F28335 or F28379D and I never saw something like this there. What is the purpose of those capacitors?
Additionally the recommended VREF capacitance is 2x2.2uF on the control card with F280049. The delfino cards show a much higher vref capacitance and even small resistor values in series. I assume to damp possible oscillations. Where does this need for such a higher capacitance come from. The analogue modules seem similar. Is it just the additional adc channels and higher adc clock?
Kind regards,
Martin