This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TIDM-1000: In the official TIDM code, the frequency and amplitude of the input voltage change. Does the code need to be modified?

Part Number: TIDM-1000
Other Parts Discussed in Thread: POWERSUITE

Tool/software: Code Composer Studio

thank you for your help,There is no parameter option for voltage amplitude and voltage frequency in the GUI. How do I choose the input voltage to be 208V/60HZ or 400V/50HZ?
In the pfc3phvienna_settings.h file, ""#define AC_FREQ 60" AC_FREQ is the frequency of the AC input? If so, can it be changed to 400HZ?
Looking forward to your reply, thank you!