Part Number: TMDSHVMTRPFCKIT
Hello,
I wanted to post this question in motor driver forums, but I couldn't. So I will ask it here.
I am using TMDSHVMTRPFCKIT to run a 200V PMSM. I have used my own FOC code with other drivers such as BoostXL-DRV8305 with lower voltage of 50V and it works fine. Now that I am using higher voltage the motor gets very hot immediately. I have connected the Kit to 110V AC so my DC bus is 160V, I have even saturated Vd and Vq to values such as 20V, but still the motor gets very hot. What can be the issue here?
Regards,
Ata