Hi,
We are beginning a new hardware design that involves:
1. 10/100 Ethernet
2. Many channels of 16-bit resolution ADCs
3. Should have in-built second order low pass filter in each channel.
4. A small footprint RTOS as suitable for selected micro controller.
I have seen the details for TMS320F28386S but the part is still in development phase and not available in Digikey.
The TMS320F28386S has got features like 10/100Mbps ethernet and 16-bit resolution ADC channels.
Any body please assist me in the correct microcontroller part selection with the main features as listed above.
Thanks,
Nagendra