This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Max ePWM frequency on F28388 vs older parts

Part Number: TMS320F28388D


Hi,

Chapter 3.7.3.3 of the F28388 TRM (SPRUII0) states that "the ePWM clockl each have an additional /2 divider, which is required to support CPU frequencies over 100MHz". However the datasheet states that the ePWM and HRPWM work with frequencies up to 200MHz. 

Can someone confirm that the ePWM modules do work up to 200MHz?

Thanks,

Pierre