Dear Team,
Hope you are doing well. I extremely need your kind help. I am working with TIEVM-HV-1PH-DCAC as a grid connected inverter. The device has been set up for 60 Hz, 110 Vrms and 380 Vdc by default and it probably works. However, I need to operate the inverter in 50 Hz. I have tried a lot to design a suitable controller for this case (based on the fact that I cannot change the LCL filter). However, due to the effect of active damping of inverter (notch filter at filter's resonant frequency), I could not design a suitable controller. is there any default controller for 50 Hz for any rated power and input output voltage? If yes, How can I have it?
Many thanks in advance for your help.
Best Wishes