Part Number: DRV8301-HC-C2-KIT
Hello,
1. I just have received DRV8301-HC-C2-KIT and set the SW3 UP and launched "InstaSPIN-BLDC_GUI_DRV83xx_v104.exe"
It shows "Connection could not be established (exception)".
2. Suspected program in the Piccollo, and launched CCS.
Created new configuration and loaded "InstaSPIN-BLDC_GUI_DRV8301_v104.out", which was successful.
3. Before exit CCS, connection was tested.
When SW3 is up, it is failed. When SW3 is down, the connection test was successful.
4. CCS was installed with all the library and tools for C2000 and Windows says that the device driver is properly working.
So, I believe what I did is not incorrect.
However, "InstaSPIN-BLDC_GUI_DRV83xx_v104.exe" still shows error "Connection could not be established (exception)".
SW3 was set UP. Of course, I tested both of UP and DOWN.
Please help.
Thanks in advance,
Heon Lee