Part Number: DRV8312-69M-KIT
Tool/software: Code Composer Studio
I've the DRV8312-69M-KIT and I tested the BLDC sensorless Firmwares
1- Instaspin-FOC
2- Controlsuite/~/BLDC-Sensorless
But eventually I need to migrate to TMS320F2812 for Down-hole operation, so my questions are:
1- which firmware from the above is applicable to work with the target MCU (even after Firmware modification not hardware issue)
2- if both can't, is there's any BLDC firmware to test on TMS320F2812
3- is PID_GRANDO library can work with TMS320F2812 (or recommend PID library equivalent)
Thanks