Other Parts Discussed in Thread: C2000WARE
Customer asks:
1. Have you test discharge mode? It is seems that there isn’t source code for discharge mode in this project.
2. For synchronous rectification(Function CLLLC_HAL_setupSynchronousRectificationAction()), where enable the Trip-Zone?
3. Line 193 in CLLLC.C file, the calculation of “CLLLC_vSecSensed_Volts” is base on “CLLLC_VSEC_OPTIMAL_RANGE_VOLTS”,
why is not “CLLLC_VSEC_MAX_SENSE_VOLTS”?
4. Two current scaling calculation results in schematic(“77.7mV/1A” and “20mV/1A” in the red circle), are they correct? How