What the meaning of the sentence "This pin has an internal pulldown and should never be pulled high"? Is that means /TRST can‘t been high?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kang,
Can you give the literature # for the document where you foudn this note, or just the download URL? This note is incorrect/incomplete.
The closest I can find to this is in the datasheet, in the pin description for TRSTn(link below). I beleive this definition is more clear, but I'd like to make sure that your example gets corrected.
What the note should say is that this pin should remain low during during normal operation. When debugging the device the signal will be driven high by the JTAG emulator. There are also some boundary scan modes that can be activated when pulling this high in conjuction with the state of EMU0/1.
Best,
Matthew