Other Parts Discussed in Thread: C2000-GANG,
Dear team,
My customer is using F28M35H52C and C200-GANG. The Memory Option in the C2000-GANG software supports only 0x681000 - 0x68101F for the 28M35H52C OTP programming address range.
But i checked the datasheet and users guide,It showed that the start address of OTP is 0x680800.
In C:\ti\controlSUITE\device_support\f28m35x\v207\MWare\cmd, it also showed like the following
OTPSECLOCK : origin = 0x00680800, length = 0x0004 OTP_Reserved1 : origin = 0x00680804, length = 0x0004 OTP_Reserved2 : origin = 0x00680808, length = 0x0004 OTP_Z2_FLASH_START_ADDR : origin = 0x0068080C, length = 0x0004 OTP_EMACID : origin = 0x00680810, length = 0x0008 OTP_Reserved3 : origin = 0x00680818, length = 0x0004 CUSTOMER_OTP_MAIN_OSC_CLK_FREQ : origin = 0x0068081C, length = 0x0004 OTP_Reserved4 : origin = 0x00680820, length = 0x0004 OTP_BOOT_MODE_GPIO_CONFIGURE : origin = 0x00680824, length = 0x0004 OTP_Reserved5 : origin = 0x00680828, length = 0x0004 OTP_ENTRY_POINT : origin = 0x0068082C, length = 0x0004 OTP_Reserved6 : origin = 0x00680830, length = 0x0010
Please help.
BR,
susan