Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: TMS320F28377D reset IC TPS3702

Part Number: TMS320F28377D
Other Parts Discussed in Thread: TPS3702

Hi,

TMS320F28377D recommend voltages are  "1.14V<VDD<1.26V" and "3.14V<VDDIO<3.47V",

Controlcard uses TPS3702CX33 and TPS3702CX12,

They monitor  voltages may be  3.0V<TPS3702CX33<3.6V and  1.09V<TPS3702CX12<1.25V .

Is there any risk when "1.09V<VDD<1.14V" , "1.25V<VDD<1.26V" , "3.00V<VDDIO<3.14V", "3.47V<VDDIO<3.60V"?

thanks,

TPS3702:

best regards,

Simen