This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: CAN message ID's

Part Number: TMS320F28379D

Hi everyone,

i'm using the C2000 Launchpad XL to receive and transmit messages via CAN.

The problem i'm facing is the possible message ID's. I set up message boxes as follows;

CAN_setupMessageObject(CANB_BASE, CO_MSG_OBJ_ID_RX_TPDO1, CO_COB_ID_TPDO1,
CAN_MSG_FRAME_STD, CAN_MSG_OBJ_TYPE_RX, CO_COB_ID_T_MASK,
CAN_MSG_OBJ_RX_INT_ENABLE | CAN_MSG_OBJ_USE_ID_FILTER,
CO_MSG_DATA_LENGTH_TPDO);

Note: 

CO_MSG_OBJ_ID_RX_TPDO1 = 21

CO_COB_ID_TPDO1 = 0x180

CO_COB_ID_T_MASK = 0xF80

And i can get messages from different nodes 0x181, 0x182, 0x183... 

But when i read the coming data with function, I only know object ID (21, 22, 23 etc.). I can not get message id. 

I'm using C2000 Ware drivelib. How can i find which message id (node id) came?