This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TMS320F2808: Device selection

Intellectual 1710 points

Replies: 1

Views: 107

Part Number: TMS320F2808

Hello, 

To help make decision on a suitable device for our product, We have a few questions we need support to answer;

1)      The F2801, F2808, F2812 and F2407A are classed as ‘other real-time control MCUs’.  They appear to be legacy devices. I read (somewhere) that the 2801, 2808 and 2812 are not recommended for new designs, although they are still classed as ‘active’ parts. But what about the F2407A?

2)      Are the ‘other  real-time MCUs’ still compatible with the latest development suites?

3)      Is there an objective argument why I shouldn’t be using these ‘other  real-time MCUs’ in future designs?

5)      Are the F28035 and F28335 both ‘Gen2’ devices, and the F28377D a ‘Gen3’ device? What were the release dates of the F28035, F28335 and F28377D? as We need to choose a future-proof device.

6)      The F28335. I don’t see any reference to comparator features (COMP/CMPSS). Is this true?

A question about IntraSPIN-FOC and IntraSPIN-MOTION.

7)      Are IntraSPIN-FOC and IntraSPIN-MOTION available the devices listed in blue in the table above? Are they hardware features or software features? And if software, what hardware is needed to run them?

And  about peripherals

8)      Some peripherals appear to be mutually exclusive? Is there a some sort of tool that allows me to allocate peripheral functions for a particular device, and see what is still available. I’d rather not have to dig into a 2500 page datasheet only to find half way through that I can’t have both SPI and I2C on a particular a bank (crude example possibly not applicable).

And a general question

9)      What is the US export control status of the three parts in blue above? ITAR? Department of Commerce? No restrictions?

Hoping you are able to answer these questions.

Many thanks

Linda

  • 1. The older F28x are still recommended, but there are usually better choices available from the newer portfolio for new designs. LF240x was recently moved from NRND back to Active due to new TI policy, but I would not start a new design.

    2. LF24x are not supported in latest CCS.  F28x are.  Older F28x are, but may only have example SW from older controlSUITE and not C2000Ware

    3. If you have a design done with them you should feel confident going to production and having supply. If starting a new design, I would look at newer devices.

    5. Yes. Off the top of my head. F2833x - 2007; F2803x - 2009; F2837x - 2014

    6. Correct

    7. I don't see a table. InstaSPIN-FOC is on F2802x, F2805x, F2806x, F28004x. InstaSPIN-MOTION on F2805x, F2806x

    8. There is a PINMUXTOOL

    9. I don't see a table, but almost all of our devices are 3A991A2 or EAR99

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.