Other Parts Discussed in Thread: TMS320F2812
I am designing a board that will use the TMS320F2812 to
control a power supply. It it critical to prevent pins
attached to power devices from glitching, especially during
power up.
With other micros, I had merely to find what state the
digital outputs assume while the RESET input is true, and
make that state 'OFF'. For the F2812 I can find little info
on this, but section 6.9 of the _Data_Manual_ (SPRS174Q)
contains the language:
"The GPIO pins are undefined until Vdd = 1 V and
Vddio = 2.5 V."
"Undefined" is not "defined" anywhere, but I interpret this
to mean:
- They might be inputs, (and tri-stated),
- They might be outputs, and high,
- They might be outputs, and low, or
- They might play the entire second movement of Beethoven's
9th Symphony at a frequency only dogs can appreciate.
Thus, if I want to protect my output devices from damage, I
must install a hardware-controlled gate layer between the
micro and its application circuit to prevent power-up
glitches. (This is a major disappointment, as the F2812
costs 3x as much as the 8-bit micro that doesn't need such
countermeasures.)
Am I missing anything?
============================================================
Gary Lynch printf("lynchg%cstacoenergy%ccom", 64, 46)
============================================================