I have a BLDC motor, it has 3 hall sensors in 120 degree position. i tested hall sensor sequence is: 110,010,011,001, 101,100, and in reverse direction, the hall sensor sequence is 001,011, 010,110,100, 101. pls help check if these sequence are correct or not?
if the hall sensor sequence is correct, what PWM sequence I need to give to the motor in both direction?
thanks