Other Parts Discussed in Thread: LAUNCHXL-F28027
Hi,
I m having a schematics based on TIDA01292
I m getting the following error :
Error connecting to the target:
(Error -1015 @ 0x0)
Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 8.0.27.9)
I did check device connection - it says JTAG integrity scan test failed
the XRSn signal is not low, TRSTn signal changes levels when usb is plugged in and the TEXAS instrument probes are visible in device manager, no brown out issue also checked all voltage levels, What else can be the issue??
Please help, the board has to go for production i m facing this basic issue, i m unable to resolve it