Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
Hello,
I'm using the LAUNCHXL-F28379D device in my embedded system.
I'm not powering the device via USB interface, instead I used dedicated DC-DC converter has 3.3V output.
In addition to that, I want the device to boost 3.3V to 5V internally. Therefore, i will remove jumpers JP1 and JP2 and i'm going to assemble JP6.
First of all, could you please confirm my above application?
Second, here a question rises. I'm also planning to use SCIBRX and SCIBTX signals in order to communicate with device as shown below. I want to know the output and input signal levels whether they are 3.3V referrenced or 5V.
Could you please inform about this issue?
Third one and last, if I use below configuration as photo.
Consequently, how can i know the signal voltage levels whether they are 3.3V or 5V leveled such as
1) PWM outputs,
2) ADCIN14,ADCINC3,ADCINB3,..ADCINB2
3) GPIO ports like P124,P124,P58,P59
Actually, I showed in box as below as a summary
Thank you.