Part Number: TMS320F280049
Other Parts Discussed in Thread: TMS320F28388D
Hello Support team.
I have a question related to security of F280049 device.
Question is about when system needs to disable JTAG in the product version.
I checked TRM and I found the below description.
However, I would like to know if F280049 can disable JTAG port simply.
=====
3.13.1 Functional Description
The security module restricts the CPU access to on-chip secure memory and resources without interrupting or stalling CPU execution. When a read occurs to a secure memory location, the read returns a zero value and CPU execution continues with the next instruction. This, in effect, blocks read and write access to secure memories through the JTAG port or external peripherals.
・
・
• Flash Sectors: Flash sectors of both the banks (Bank0 and Bank1) can be made secure on this device. Each Flash sector can be allocated to either zone by configuring the respective GRABSECT location in the respective bank's USER OTP.
=====
Best Regards
KORO