Hi, One
There's one doubt about HRPWM.
PWM5 and PWM6 are used:
1) High resolution, CMPA, CMPB, TBPRD
2) PWM6 is linked to PWM5 with CMPA, CMPB, TBPRD and GLDCTL2.
3) PWM5 sends SYNC to PWM6
The doubt are:
1) PWM5 global load is used, does PWM6 need to use?
2) PWM6 registers are linked to PWM5. At the moment PWM5 CMPA changed, when will PWM6 CMPA be changed? By shadow, or immediately?
3) Is there any restriction on these kind of configuration? We found that, when global load is used, PWM6A sometimes doesn't work well, but PWM6B can work well.
Thanks a lot.
Br, Jordan