Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, TPS62162
Hi community!
I want to connect a 5V external source to the LAUNCHXL-F28379D board to support my own interface (e.g., encoder, LEDs mounted on an external board).
It is mentioned in User's Guide that for doing so, I have to remove JP2, JP3, and JP6. However, removing JP2 isolates the ground of the external 5V from the USB ground. Is it correct? Shouldn't I connect these two grounds to each other for proper functioning of the board?
Besides, in schematic design files given in C2000, there is a 0 ohm resistor (R25) in parallel with JP2 ! But I can't find it on the launchpad board. Is this resistor really exists?
Regards