Customer wants to use internal ADC reference and AIO functions in F28035. Could you please help address the below questions?
1. How about the performance of internal ADC reference?
I only found the below spec regarding the internal reference: Overall gain error and ADC temperature coefficient.
The ambient temp range for their application is about -25~85C, and in some critical conditions, they need to consider -40~105C. Is there any concern about the temp drift? Besides, as for the accuracy, is there any spec defined? Also, I wonder whether its accuracy is related to the accuracy of the 3.3V VDDA supply.
2. AIO usage
a. Does using AIO as output have less cross-talk effect for adjacent analog signals, compared to using AIO us input?
b. Note that it is not suggested to use AIO with high frequency toggling, so is it okay to use it for 2KHz output signal to control LED?
c. Is there any extra delay to use AIO as a status indicator(input), compared to GPIO?
Highly appreciated with your feedback!