Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Hii,
I am trying to generate SVPWM using LAUNCHXL-28379D. The progem run successfully without any error but it shows me an error during debug. The error are shown below:
C28xx_CPU1: Error adding memory map range: invalid page specified
C28xx_CPU1: Error adding memory map range: invalid page specified
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1LINKPOINTER1"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1LINKPOINTER1"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1LINKPOINTER2"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1LINKPOINTER3"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1PSWDLOCK"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1CRCLOCK"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1OTPBOOTCTRL"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1GRABSECT"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1GRABRAM"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1EXEONLYSECT"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z1EXEONLYRAM"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2LINKPOINTER1"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2LINKPOINTER1"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2LINKPOINTER2"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2LINKPOINTER3"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2PSWDLOCK"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2CRCLOCK"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2OTPBOOTCTRL"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2GRABSECT"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2GRABRAM"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2EXEONLYSECT"
C28xx_CPU1: Error occurred during flash operation: Unknown property "Z2EXEONLYRAM"
C28xx_CPU1: Error occurred during flash operation: Unknown property "FlashCoreSelection"
C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
C28xx_CPU1: Flash Programmer: Missing Flash Programming Settings.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: C:\Users\HP\workspace_v6_1\adc_soc_epwm_cpu01\CPU1_FLASH\adc_soc_epwm_cpu01.out: Load failed.
Please suggest me where the problem is.