Other Parts Discussed in Thread: C2000-GANG
Hi team,
Here is a problem I met when supporting customer flash F2802 with C2000-Gang.
1. When they use production tool board with 20Mhz oscillator to flash F2802, if they select 20Mhz DSP clock, an error would happen:
Error 70: DSP CLK frequency error
If they select 40Mhz, the device can be flashed. But if they try to flash the device again, it would show:
Error 69: DSP Firmware start;
Error 70: DSP CLK frequency error
2. If they use the same board and flash the device with CCS, everything runs well.
3. When they use official PCB board also with 20Mhz oscillator to flash F2802, if they select 20Mhz DSP clock, the error never happened.
Any idea what is happening here? What does the DSP clk in C2000-GUI represent? And what is the right value to set?
Regards,
Brian