Other Parts Discussed in Thread: INA240
There are missing xBar output TripIN defines (xbar.h) shown in two TRM tables as TripIN-1-12
TRM Fig. 9-5/18-57 are drawn incorrectly according to other tables. Table 9-2 shows Mux 0-31 with CMPSSn.CTRIPH_OR_CTRIPL via xBAR outputs into combinational, shown 18.11 DC sub module Fig.18-48. TripIN 1-12 have missing defines for several shown in Fig.9-5. So XBAR_setEPWMMuxConfig() and XBAR_enableEPWMMux() can not assign some TripINx shown Mux table 9-2 via xbar.h limited defines.
Where are XBAR_Trip1, 2, 3, 6 shown in table 9-2? Seemingly the xBAR outputs (Fig.18-48) have to match Mux table (9-2) CMPSSn (verbatim) leading into the DC trip module. It seems HW forces to use TripIN1 for CMPSS1 into combinational trip control shown in Fig.18-48. Plausible someone got MUX defines confused with TZ1-3, 6 as OMG there are so many routes to take.