Hi all,
According to datasheet, when we select Flash/USB boot mode and when the default flash entry address is unprogrammed will switch the boot mode to USB boot.
My question is that in a programmed device, when software receive the firmware upgrade command, can we use software erase the default flash entry address, WD reset and then F28384D switch boot mode to USB boot again? It means that customers can use this method and always do software upgrade via USB port.
Another question, the default flash entry address is 0x00080000, is it correct?
Regards,
Luke