Other Parts Discussed in Thread: UNIFLASH, CONTROLSUITE, F28M36P63C2
Hello,
Having an issue uploading example software to the TMDSDOCK28M36 for the first time.
Using Code Composer and default board settings I was able to verify the internal s100v2 connection in the property window. When clicking the debug button to upload the project, I get stuck on the GEL expression - OnTargetConnect() and eventually cancel because too much time has passed.
According to the Errata of the R1.1 Version 1.3 May 2016 of the TMS320F28M36 Concerto controlCARD R1.1 Information Guide document
It can be difficult to connect to the MCU via JTAG when using the Boot-to-Flash boot mode if no code is already loaded into the device. It is recommended to use Boot-from- Ethernet boot mode (or other boot mode) until valid code is loaded into FLASH.
With this information I have tried to switch board settings and use the UNIFLASH application to upload to the board.
The SW1 is set to serial peripherals 0010 before powered up
A:SW1 position 2 need to set to ON to enable internal FTDI USB to serial
A:J1 USB connection is made to the computer. (no additional USBs or power connected)
UNIFLASH detects the internal s100v2 but fails to upload
Texas Instruments XDS100v2 USB Debug Probe/IcePick_C_0
Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)
Changing the A:SW1 position 1 to off so it disables the s100v2 and starting the process over using UNIFLASH failed again.
I would ultimately like to successfully run the F28M36x example for lwip located here in control suite here:
C:\ti\controlSUITE\device_support\f28m36x\v220\F28M36x_examples_Master\enet_lwip\m3\ccs