This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377D: F2837xD_Adc CCS 20v compiler issue

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE

Tool/software: TI C/C++ Compiler

Dear TI Hello,

I am using the last version of the C2000Ware and I have this issue while compiling project using the last compiler,

----------------------------------------------------------------------------------------------------------------------------------------------------------

Building file: "C:/ti/c2000/C2000Ware_3_01_00_00/device_support/f2837xd/common/source/F2837xD_Adc.c"
Invoking: C2000 Compiler
"C:/ti/ccs1000/ccs/tools/compiler/ti-cgt-c2000_20.2.0.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 --include_path="C:/Users/Usr/Desktop/TS_F28377D/01_TS_GPIO" --include_path="C:/ti/ccs1000/ccs/tools/compiler/ti-cgt-c2000_20.2.0.LTS/include" --include_path="C:/ti/c2000/C2000Ware_3_01_00_00/device_support/f2837xd/common/include" --include_path="C:/ti/c2000/C2000Ware_3_01_00_00/device_support/f2837xd/headers/include" --include_path="C:/ti/c2000/C2000Ware_3_01_00_00/driverlib/f2837xd/driverlib" --include_path="C:/ti/c2000/C2000Ware_3_01_00_00/driverlib/f2837xd/driverlib/inc" --include_path="../TS_SysMng/Inc" --advice:performance=all --define=_DUAL_HEADERS --define=_LAUNCHXL_F28379D --define=_FLASH --define=CPU1 -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=coffabi --preproc_with_compile --preproc_dependency="TS_DspMng/DeviceSupport/Src/F2837xD_Adc.d_raw" --obj_directory="TS_DspMng/DeviceSupport/Src" "C:/ti/c2000/C2000Ware_3_01_00_00/device_support/f2837xd/common/source/F2837xD_Adc.c"

>> Compilation failure
TS_DspMng/DeviceSupport/Src/subdir_rules.mk:9: recipe for target 'TS_DspMng/DeviceSupport/Src/F2837xD_Adc.obj' failed

INTERNAL ERROR: C:\ti\ccs1000\ccs\tools\compiler\ti-cgt-c2000_20.2.0.LTS\bin\ac2000.exe experienced a segmentation fault
while processing function (unknown or file scope) file (unknown) line 0

This is caused by a defect in the TI C/C++ Parser.
TI Customer Support may be able to suggest a workaround to avoid this.

Upgrading to the newest version of the compiler may fix this problem.

Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue".

We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.
Include the .pp file created by option --preproc_with_comment


----------------------------------------------------------------------------------------------------------------------------------------------------------

Could help me resolve this problem please, should I told my community to use the 18v of TI compiler?

Thank you in advance,

S.Tarik,