Hi Experts,
Our customer has faced a verify error with the C2000-GANG image programming to F28075.
The procedure is as follows:
1) Developed FW is flashed onto F28075 on their board through XDS200.
2) "Read" button on C2000-GANG GUI is used to read the TXT file from the F28075 through the C2000-GANG.
3) "Copy file to Image" button is pressed to create .c2000gangbin and flash onto the C2000-GANG itself.
4) "GO" button on the C2000-GANG itself is pressed to program the image onto F28075.
5) Verify NG occurs.
In addition, it works fine with F28069.
On the other hand, if the .txt file is utilized instead of the .c2000gangbin, it works with no problem.
1) "Open Code File" is utilized to read the .txt.
2) "Save to Image" is pressed to save the file onto the C2000-GANG.
3) "GO" button on the C2000-GANG itself is pressed to program the .txt onto F28075.
4) It finishes with no problem.
The C2000-GANG version info. is attached.
Please look into it and let us know the observation.
Best regards,
Hitoshi