Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28069MISO, TMDSCNCD28069
Hello all,
I have developed a project with LAUNCHXL-F28069M. As you know "For evaluation only; not FCC approved for resale" is written on the kit.
LAUNCHXL brd files (Eagle) are given with C2000Ware and I have converted it to Altium Designer with V20 features. Its bill of material is also given.
I can design a less complicated pcb with these and adapt with my project but the pcb is 6 layer and there are lots of components. Hard work. Soldering can be difficult or not reliable enough. Mistakes can happen. I would prefer buying from you.
There is also a TMDSCNCD28069MISO controlCARD with Piccolo TMS320F28069MPZT. I havent seen a "For evaluation only; not FCC approved for resale" writing on it. For TMDSCNCD28069 F28069 Piccolo controlCARD, it is the same.
What are these control cards for exactly? About their features and programming, are they identical with LAUNCHXL-F28069M? Should I maybe use these for selling instead of not resale approved Launchxl or redesigning the pcb?
Which path do you recommend for me?