Hi Team,
I am working with a customer who is targeting synchronously sampling 3 channels differentially for a motor current measuring application. We have a few questions relating to footnote 6 in the datasheet. They interpret this as a contradict synchronous sampling and implies sampling one signal at a time. They need to measure 3 phase motor currents simultaneously. Is 3 phase simultaneous sampling possible with this device? Are you able to clarify what exactly is meant from foot note 6? I did not have the same interpretation and was hoping that this is a misunderstanding as it seems like there are enough pins to distribute the 3 simultaneous sampling signals to not cause an issue. Also are we able to quantify footnote 10 which mentions that the max DC code deviation occurs during simultaneous sampling? Appreciate your help with this!