This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: cTI 20-pin Header

Part Number: TMDSEMU110-U

Hi,

Good day, I hope everything is fine. 

Our customer was reading the "JTAG Connectors and Pinout" document [ ]

The lists of recommended or suggested parts for the Compact TI 20-pin JTAG header (cTI-20). They noticed that the suggested 3M parts, 45220-600230 and 45220-200230, do not fit the cTI-20 mate as found on, say, the XDS200. This is because their row pitch is 1.27mm, not 2.54mm.

In addition, the 3M cable side connector recommended (82020-6006RB) is correct and suitable but is in last-time buy and soon to be discontinued as they've said.

In line with this, I want to confirm if this information was correct and valid. Also, it would be helpful if you could suggest a different part number from the same manufacturer that would fit in these requirement.

I hope to hear from you soon. 

Thank you and have a great day. 


Regards, 

Cedrick