Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: TIDA-00364
Dear team:
I want to use LAUNCHXL-F28069M and TIDA-00364 for my design. The Switching Frequencies of TIDA-00364 is up to 10 kHz, So I modified the frequency of PWM in Lab01 as below:
#define USER_PWM_FREQ_kHz (8.0) //(45.0)
But after I modified, The program doesn't seem to be running (It runs normally in 45KHz). PWM port has no waveform output. Even the LED doesn't blink.
1. Can I use a PWM frequency of 8kHz to driver TIDA-00364?
2. Does instaSPIN algorithm have to connect current sampling signal? If yes, there seams no current sampling circuit in TIDA-00364, Do you have current sampling circuit design for reference?
Best regards