This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV8301-69M-KIT: DRV8301-69M-KIT

Prodigy 130 points

Replies: 1

Views: 47

Part Number: DRV8301-69M-KIT

How much variation / tolerance (in percentage) can be acceptable in the inductance value(Ls/Ld) for BLDC motor.

Thanks,

Vivishekh

  • That depends on the required motor control performance, so there is not a detailed specification. In most cases, less than 10% tolerance is ok for spinning a motor smoothly. Actually, the inductance of the motor will change with the current increase.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.