Other Parts Discussed in Thread: C2000WARE
Hello Champs,
For missing clock detection logic and related configuration, is that of F28002x all the same with F28004x?
Here below is missing clock detection description from chapter 3.7.12.1 of F28002x TRM:
My questions are:
(1) The CLOCKFAIL can go high to generate TRIP events to PWM, will it trip all ePWM or user needs to configure which ePWMs should be tripped? How can user configure CLOCKFAIL and the generated TRIP events? Are there any example codes for this?
(2) When NMI interrupt is generated, what should user do in NMI interrupt ISR? Have you any suggestions for that?
(3) If NMI is not enabled and MCDSTS is always set, when will reset happen?
Would you please kindly help? Thanks!
Best Regards,
Linda