Part Number: TMS320F28388D
Hi expert,
I'd like to reset and re-run my CM core application with a code jump. But it always get into an illegal ISR. My code can be as simple as below (actually I can reproduce the error on every TI example code and TI EVM).
void runImage(void)
{
void (*x)(void);
x = (void (*)(void)) 0x00200000;
(*x)();
}
//
// Main
//
void main(void)
{
volatile uint32_t delay;
CM_init();
while(1){
GPIO_writePin(DEVICE_GPIO_PIN_LED2, 0);
DEVICE_DELAY_US(500000);
GPIO_writePin(DEVICE_GPIO_PIN_LED2, 1);
DEVICE_DELAY_US(500000);
GPIO_writePin(DEVICE_GPIO_PIN_LED2, 0);
DEVICE_DELAY_US(500000);
GPIO_writePin(DEVICE_GPIO_PIN_LED2, 1);
DEVICE_DELAY_US(500000);
GPIO_writePin(DEVICE_GPIO_PIN_LED2, 0);
DEVICE_DELAY_US(500000);
GPIO_writePin(DEVICE_GPIO_PIN_LED2, 1);
DEVICE_DELAY_US(500000);
runImage();
}
}
I am using CMD file as attached:
MEMORY
{
/* Flash sectors */
CMBANK0_RESETISR : origin = 0x00200000, length = 0x00000008 /* Boot to Flash Entry Point */
CMBANK0_SECTOR0 : origin = 0x00200008, length = 0x00003FF8
CMBANK0_SECTOR1 : origin = 0x00204000, length = 0x00004000
CMBANK0_SECTOR2 : origin = 0x00208000, length = 0x00004000
CMBANK0_SECTOR3 : origin = 0x0020C000, length = 0x00004000
CMBANK0_SECTOR4 : origin = 0x00210000, length = 0x00010000
CMBANK0_SECTOR5 : origin = 0x00220000, length = 0x00010000
CMBANK0_SECTOR6 : origin = 0x00230000, length = 0x00010000
CMBANK0_SECTOR7 : origin = 0x00240000, length = 0x00010000
CMBANK0_SECTOR8 : origin = 0x00250000, length = 0x00010000
CMBANK0_SECTOR9 : origin = 0x00260000, length = 0x00010000
CMBANK0_SECTOR10 : origin = 0x00270000, length = 0x00004000
CMBANK0_SECTOR11 : origin = 0x00274000, length = 0x00004000
CMBANK0_SECTOR12 : origin = 0x00278000, length = 0x00004000
CMBANK0_SECTOR13 : origin = 0x0027C000, length = 0x00004000
C1RAM : origin = 0x1FFFC000, length = 0x00002000
C0RAM : origin = 0x1FFFE000, length = 0x00002000
BOOT_RSVD : origin = 0x20000000, length = 0x00000800 /* Part of S0, BOOT rom will use this for stack */
S0RAM : origin = 0x20000800, length = 0x00003800
S1RAM : origin = 0x20004000, length = 0x00004000
S2RAM : origin = 0x20008000, length = 0x00004000
S3RAM : origin = 0x2000C000, length = 0x00004000
E0RAM : origin = 0x20010000, length = 0x00004000
CPU1TOCMMSGRAM0 : origin = 0x20080000, length = 0x00000800
CPU1TOCMMSGRAM1 : origin = 0x20080800, length = 0x00000800
CMTOCPU1MSGRAM0 : origin = 0x20082000, length = 0x00000800
CMTOCPU1MSGRAM1 : origin = 0x20082800, length = 0x00000800
CPU2TOCMMSGRAM0 : origin = 0x20084000, length = 0x00000800
CPU2TOCMMSGRAM1 : origin = 0x20084800, length = 0x00000800
CMTOCPU2MSGRAM0 : origin = 0x20086000, length = 0x00000800
CMTOCPU2MSGRAM1 : origin = 0x20086800, length = 0x00000800
}
SECTIONS
{
.resetisr : > CMBANK0_RESETISR
.vftable : > CMBANK0_SECTOR0 /* Application placed vector table in Flash*/
.vtable : > S0RAM /* Application placed vector table in RAM*/
.text : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.cinit : > CMBANK0_SECTOR0
.pinit : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.switch : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.sysmem : > S2RAM
.stack : > C1RAM
.ebss : > C1RAM
.econst : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.esysmem : > C1RAM
.data : > S3RAM
.bss : > S3RAM
.const : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
MSGRAM_CM_TO_CPU1 : > CMTOCPU1MSGRAM0, type=NOINIT
MSGRAM_CM_TO_CPU2 : > CMTOCPU2MSGRAM0, type=NOINIT
MSGRAM_CPU1_TO_CM : > CPU1TOCMMSGRAM0, type=NOINIT
MSGRAM_CPU2_TO_CM : > CPU2TOCMMSGRAM0, type=NOINIT
.TI.ramfunc : {} LOAD = CMBANK0_SECTOR0 | CMBANK0_SECTOR1,
RUN = S0RAM | S1RAM | S2RAM,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
Could you help me with how to do this? I am not sure why error happens. We are testing this to build a user bootloader.
Thanks
Sheldon
void runImage(void){ void (*x)(void); x = (void (*)(void)) 0x00200000; (*x)();}
//// Main//void main(void){ volatile uint32_t delay; // // Initialize device clock and peripherals // CM_init();
// Synchronize both the cores. // IPC_sync(IPC_CM_L_CPU1_R, IPC_FLAG31);
IPC_waitForFlag(IPC_CM_L_CPU1_R, IPC_FLAG31); while(1){ GPIO_writePin(DEVICE_GPIO_PIN_LED2, 0); DEVICE_DELAY_US(500000); GPIO_writePin(DEVICE_GPIO_PIN_LED2, 1); DEVICE_DELAY_US(500000); GPIO_writePin(DEVICE_GPIO_PIN_LED2, 0); DEVICE_DELAY_US(500000); GPIO_writePin(DEVICE_GPIO_PIN_LED2, 1); DEVICE_DELAY_US(500000); GPIO_writePin(DEVICE_GPIO_PIN_LED2, 0); DEVICE_DELAY_US(500000); GPIO_writePin(DEVICE_GPIO_PIN_LED2, 1); DEVICE_DELAY_US(500000); runImage(); }