This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DRV8301-69M-KIT: DRV8301-69M-KIT

Prodigy 130 points

Replies: 1

Views: 40

Part Number: DRV8301-69M-KIT

On what bases SpinTAC MOVE / SpinTAC CTRL choses the cfg_AXISID as 0 / 1. 

  • Keep setting the same value in a project as the default number, ST_AXIS0 if there is only a motor.  ST_AXIS1 is for another motor if the system supports dual motor as the lab12c.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.