Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSHSECDOCK, TMDSCNCD28388D, C2000WARE
Hi I have.
TMDSCNCD28388D and TMDSHSECDOCK
I have the example led_ex1_c28x_cm_blinky_cpu1 and led_ex1_c28x_cm_blinky_cm
from C2000Ware_3_01_00_00
Both Led's are blinking when debugging.
Now I build both projects with Flash configuration. Download it via CCS and the onboard XDS100v2 Debugger.
The power is turned off and i changed S1:A from right to left on the ControlCard, then the power is turned on
and I can see no Led blinking.
What can i do ?