Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
I am having some trouble with changing the PM_tformat_lib_23789x.lib for the position manager program for the boostxl card.
Using PM_tformat_lib source in ti/c2000/c2000Ware_motorCpontol_SDK_3_00_01_00/libraries/position_sensing, I change the pm_tformat_source.c to (theoretically) do what I want but when I run the tformat_f28379x_boostxl_posmgr_site2 in the same file system, I can see that it is running some code other than the library I created.
It seems to me that I have looked in every file in the project for links, etc but they all 'appear' to point at the library I created, yet it can't be.
What am I missing? Is the process I am using to change the library correct?
Any suggestions?