Hi, All,
As the function block of TMS320F28375S,it has six pins for eCAP,,
but.....
Which pins number are eCAP pins ? does anyone know ?
BR,
Vincent.Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, All,
As the function block of TMS320F28375S,it has six pins for eCAP,,
but.....
Which pins number are eCAP pins ? does anyone know ?
BR,
Vincent.Chen
Hi Vincent,
eCAP is input pin and it is routed via INPUT XBAR to eCAP modules (please refer "Figure 9-1. Input X-BAR" in device TRM) . So you should be able to configure INPUT XBAR to connect any input pin to respective eCAP module.
Regards,
Vivek Singh
Hi, Vivek Singh,
Thank you, I have found the "Figure 9-1" in TMS320F28375S Technical Reference Manual ,but it still does not show the pin number about "eCAP",
Could you please provide the hardware pin number of eCAP ? thanks a lot.
BR,
Vincent.Chen
Vincent,
There is no dedicated pin number for eCAP. You can use any pin and configured the INPUT XBAR to connect that PIN to specific eCAP module.
Regards,
Vivek Singh