This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: CLB_INPUT_FILTER - Edge Detection

Part Number: TMS320F28379D

Greetings,

I have a question about the behavior of the edge detection capabilities which are controlled by the CLB_INPUT_FILTER register.  When one of the edge detection values is programmed, and the appropriate edge occurs, is the output a single pulse?  In other words, if a signal, which is basically DC but has a single edge in it occurs, will the output of the synchronizer (input to the tile) be a pulse to indicate that the edge occurred?

Thank you,

Ed