I am currently evaluating a
TI LaunchPad Kit C2000 Piccola F28004x
I have imported the TIDM-DC-DC-BUCK Synchronous Buck Converter
The sample compiles and runs without any issues. I can debug and watch variables without any issues. An led blinks, so I can see the state machine is working.
When I reset the board without downloading the code again, the code doesn't appear to run (No blinking LED). I assumed this was, because the application was being loaded into ram, hence a reset would mean the code is erased.
Looking at the
f28004x_flash_lnk.cmd file, it looks like the code is being run from flash. The compile flags also has _FLASH set.
I have looked at sample code, which run from Ram and Flash, so at this stage I can't see a problem.
Any advise would be appreciated.