This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] FAQ: Support for using MathWorks Solutions with C2000 MCU's

Prodigy 130 points

Replies: 1

Views: 198

MathWorks Embedded Coder with the MathWorks TI C2000 Hardware Support Package allows automatic build and execution on C2000 hardware from models developed using MATLAB and Simulink.

Answers to some common advanced questions are available on TI's E2E forum:

1. How do I use Simulink “Custom Code” blocks to measure code execution time on TI C2000?

2. How do I define a Custom Memory section for a TI C2000 using MathWorks Embedded Coder's Custom Storage Class designer?

3. How do I use MathWorks Embedded Coder to load data/code to flash and run from RAM on a TI C2000?

4. What are the supported data types when designing a Simulink application for TI C2000?

5. How can I use a two model approach in MathWorks Embedded Coder for signal logging and parameter tuning on a TI C2000?

Extensive documentation about MathWorks' C2000 hardware support, including setup and a getting started video, is available on MathWorks' website (access may depend on your MathWorks login).

Additional C2000 specific questions can be posted on TI E2E. Questions specific to MathWorks products (such as MATLAB, Simulink, and Embedded Coder) can also be posted to MATLAB Answers forum or, if your license includes live support, asked directly to MathWorks' tech support

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.