Other Parts Discussed in Thread: TMDSCNCD28069MISO, TMS320F28069
I am using the TI High Voltage Motor Control Kit, TMDSHVMTRINSPIN. Few months back I was able to use the board to turn a motor. After a gap of 4 months, today I tried to use the board again to turn the motor. I set up the system as I always have. I began by connecting the 15 V power supply, then I applied the 230V AC input. I then went to connect the micro USB cable to the f2806 control card (the USB end was already connected to the computer). Much to my surprise, this caused a short circuit/spark that fried my control card and my computer. The grounding jumper was in place on the board, M3-J5 is populated, J9 (main) not populated. so I am not sure what caused this. I assume its either a ground loop or some kind of short inside the board. Is this an issue that has been experienced in the past? Any help is appreciated.