Part Number: TMS320F280048C
I'm able to boot from flash no problem using the default boot pins (GPIO 24 / 32) with GPIO32 being pulled high externally.
Down the line, I'd like to be able to boot from serial via a MAX3221 RS232 transceiver (GPIO 28 / 29) where I've connected GPIOs 24 and 28. The idea being that the inverted output in the serial driver would be enough to show a low on BOOT pin 1 when RX is high. In practice, I haven't been able to get this to boot and I always boot into flash.
Anyone have any experience pulling something like this off?