Hello,
I have a question about Simulink tool. I don’t know if some blocks does not working with TI C2000 Support Package well. I built two simple models. The first one could drive the motor well. But another couldn’t drive the motor well. I don’t know if some block or blocks doesn’t work with TI C2000 Support Package well. If I did simulation for these 2 models. The outputs were the same to hardwares. But I don’t know why the first model can spin the motor. But the second cannot. I attach the two model for you to review. I also paste 2 snapshots for output from the simulation. I really don’t if some Simulink block doesn’t work with TI C2000 Support Package well. Can you let me know if you investigate it and find some reasons? I also paste the 2 models below.
Best regards,
Hao