Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: SDRAM inquiries

Part Number: TMS320F28388D

Hi sir,

A customer have the inquiries below.

1. Does the EMIF2 CS0N of TMS320F28388D support the External of 32M SDRAM?

2. If possible, how to connect the hardware? I want to use the SDRAM of MT48LC16M16A2P。

3. Another one question is to expand NOR FLASH MT28FW02GBBA1HPC through EMIF1  CS0N, How to connect the hardware?

Thank you for your help in  advance.

  • Hi,

     1. Does the EMIF2 CS0N of TMS320F28388D support the External of 32M SDRAM?

    Yes. This is mentioned in device datasheet (Table title "EMIF Chip Select Memory Map"). Any specific reason you asked this query.

     2. If possible, how to connect the hardware? I want to use the SDRAM of MT48LC16M16A2P。

    Please refer this appnote for more detail on this.

     3. Another one question is to expand NOR FLASH MT28FW02GBBA1HPC through EMIF1  CS0N, How to connect the hardware?

    Yes, it can be done but via ASYNC interface (CS2/CS3) and not via CS0. Generally this is generic interface which can be used so we do not have any additional document for this. If you have any specific query on this, please let us know and we'll try to answer.

    Regards,

    Vivek Singh