Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Dear TI,
I want to get started with the TI example to learn about CAN in Texas Instruments DSP.
In this example "can_ex3_external_transmit". I modified the GPIO because I'm using the Launchxl board,
//! \b External \b Connections \n //! - ControlCARD CANA is on GPIO4 (CANTXA) and GPIO5 (CANRXA) //! - ControlCARD CANB is on GPIO6 (CANTXB) and GPIO7 (CANRXB)
Do these PINs CANTXA and CANRXA have to be connected to the transceiver circuit or I could run this example without an external circuit?
How I could execute this example without connecting the transceiver circuit?
Thank you in advance for the help,
S.Tarik,